could we use these sensors for measuring negative pressure of -2kPa?
Hello Marc,
The MPXx5004 family have a pressure range from 0 to 3.92kPa and not suitable for negative pressure readings as per the sensor can get damaged.
If you need to measure negative values of -2kPa or higher, we recommend the vacuum sensors below:
I hope this information can be helpful.
Have a great day,
Paulina
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------