MPXM2202

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXM2202

1,233 Views
brian_zargari
Contributor I

When using the MPXM2202GST1 or the MPXM2053GS:

1.  What does the 5th pin (tab) connects to? Can it connect to GND or should it be left unconnected?

2.  Can the "Vout-" pin be connected to GND for single ended use or does it need to be isolated from GND?

3.  What is the most common way of amplifying the 40mV full scale output to get a single ended output? Is a single stage instrumentation amplifier the answer? Is there an example schematic?

Labels (1)
0 Kudos
Reply
1 Reply

894 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Brian,

1. As for the MPAK package, it is necessary to connect only the following pins:

1 – GND

2 – +Vout

3 – Vs

4 – -Vout

The 5th pin has no internal connection, but you can provide a pad for it.


2&3. A recommended approach is to use an instrumentation amplifier to translate the sensor’s differential output into a single ended analog signal. For instance, the INA122 instrumentation amplifier is inexpensive, widely available and the only thing you need to do to set the gain is choose a gain resistor.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply