MPXH6400AC6T1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXH6400AC6T1

Jump to solution
2,692 Views
cwtengr
Contributor I

There are 4 pins that state "Do not connect to external circuitry or ground." Is it recommended to connect these DNC pins together to provide better structural strength for the sensor? Will this affect any signals? Removing tubing can sometimes cause the sensor to be ripped from the PCB.

0 Kudos
1 Solution
2,683 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

These pins must be leave unconnected since these pins are used for factory calibration, you must not connect to external circuitry or ground, otherwise you will probably change the calibrations values causing a malfunction of the device, or even worst, the device could be permanently damaged.

So, as I mentioned before, I do recommend leave these pins unconnected.

I hope this information will be useful for you. I am glad to help.

Best regards,

David

View solution in original post

0 Kudos
1 Reply
2,684 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

These pins must be leave unconnected since these pins are used for factory calibration, you must not connect to external circuitry or ground, otherwise you will probably change the calibrations values causing a malfunction of the device, or even worst, the device could be permanently damaged.

So, as I mentioned before, I do recommend leave these pins unconnected.

I hope this information will be useful for you. I am glad to help.

Best regards,

David

0 Kudos