MPX5010 vs MPX2010

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPX5010 vs MPX2010

2,143 次查看
jasonhaedt
Contributor III

Dear Freescale,

I currently use MPX2010 in a dual port configuration.  I am looking to move to the MPX5010 with the integrated amplifier but had a few questions:

1.) Is the sensor the same in the MPX2010 and the MPX5010?

2.) Are there any application recommendations for interfacing to the MPX5010?

Sincerely,

Jason

标签 (2)
0 项奖励
回复
1 回复

1,773 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Jason Haedt,

Answering to your questions:

  1. It is a very similar sensor with the difference (that you already noticed) that the MPX5010 is on-chip amplified, but both have the same pressure range and general functionality.

  1. It is actually very simple to interface the MPX5010 since it’s already amplified, temperature compensated and calibrated, so the only think you need to add are just a few capacitors (as seen on Figure 3 of the datasheet) and the signal goes directly to your mcu’s ADC.

Click here to find all the documentation available for the MPX5010.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复