I have the MPX4115AP sensor. I have it hooked up according to you datasheet. The output of Pin 1 (Pin 3 is +5V) starts at 3.8V when power is first applied, and then drops gradually to about 2.5V after 5-10 seconds. The air pressure is not changing.
When I do change the air pressure, however, the reading continues to drop - it has no effect.
Any help would be appreciated (and the sooner the response the better)!
Thanks!!!
解決済! 解決策の投稿を見る。
Hello Mark,
Yep, you're rigth... I'll ask the appropriated persons to take a look at the dates on the forums. Perhaps Carlos might help 4guin4g4 ?
Well, at least he had an answer from us =).
Cheers,
Josh
Hello Ian,
Could you please let me know what is the specific part number of the device that you're using? There are two datasheets for this device (depending on the device version), both of them shows the pin out as follows:
pin#1: NC
pin#2: Vs
pin#3: GND
pin#4: Vo
MPXAZ4115A Series:
http://cache.freescale.com/files/sensors/doc/data_sheet/MPXAZ4115A.pdf
MPXV4115V Series:
http://cache.freescale.com/files/sensors/doc/data_sheet/MPXV4115V.pdf
Regards,
Josh
Hi Josh,
Something is wrong with the dates on this board. I believe Ian asked that question more than 5 years ago.
The board shows he asked the question on October 1 of this year, but that Alban responded back in 2007. The June 2007 date is correct, so I would hope that Ian is not still waiting on an answer.
Hello Mark,
Yep, you're rigth... I'll ask the appropriated persons to take a look at the dates on the forums. Perhaps Carlos might help 4guin4g4 ?
Well, at least he had an answer from us =).
Cheers,
Josh
I will take a look at the migration of the dates..