MPX4115AP weird reading

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPX4115AP weird reading

跳至解决方案
3,137 次查看
Ghost13
Contributor I

I have the MPX4115AP sensor. I have it hooked up according to you datasheet. The output of Pin 1 (Pin 3 is +5V) starts at 3.8V when power is first applied, and then drops gradually to about 2.5V after 5-10 seconds. The air pressure is not changing.
When I do change the air pressure, however, the reading continues to drop - it has no effect.

Any help would be appreciated (and the sooner the response the better)!

Thanks!!!

标签 (1)
标记 (1)
0 项奖励
1 解答
2,130 次查看
Joshevelle
Senior Contributor I

Hello Mark,

Yep, you're rigth... I'll ask the appropriated persons to take a look at the dates on the forums. Perhaps Carlos might help 4guin4g4 ?

Well, at least he had an answer from us =).

Cheers,

Josh

在原帖中查看解决方案

0 项奖励
5 回复数
2,130 次查看
Joshevelle
Senior Contributor I

Hello Ian,

Could you please let me know what is the specific part number of the device that you're using? There are two datasheets for this device (depending on the device version), both of them shows the pin out as follows:

pin#1: NC

pin#2: Vs

pin#3: GND

pin#4: Vo

       

MPXAZ4115A Series:

http://cache.freescale.com/files/sensors/doc/data_sheet/MPXAZ4115A.pdf

MPXV4115V Series:

http://cache.freescale.com/files/sensors/doc/data_sheet/MPXV4115V.pdf

Regards,

Josh

0 项奖励
2,130 次查看
rocco
Senior Contributor II

Hi Josh,

Something is wrong with the dates on this board. I believe Ian asked that question more than 5 years ago.

The board shows he asked the question on October 1 of this year, but that Alban responded back in 2007. The June 2007 date is correct, so I would hope that Ian is not still waiting on an answer.

0 项奖励
2,131 次查看
Joshevelle
Senior Contributor I

Hello Mark,

Yep, you're rigth... I'll ask the appropriated persons to take a look at the dates on the forums. Perhaps Carlos might help 4guin4g4 ?

Well, at least he had an answer from us =).

Cheers,

Josh

0 项奖励
2,130 次查看
4guin4g4
Contributor IV

I will take a look at the migration of the dates..

0 项奖励
2,130 次查看
Ghost13
Contributor I
No suggestions?!?!?!
:smileysurprised: :smileysad: :smileymad:
:smileyindifferent:
0 项奖励