Hi Joshevelle and thank you for your quick reply.
My application is air pressure switch. I am using at the moment the MPXM2053GS which has a comparable pressure range (0 to 50 Kpa).
The MPXM2053GS has a nice nozzle which can be connected to a hose/tube.
I am happy with the performance of the MPXM2053GS but in mass production it would be more beneficial if there is a comparable sensor at a lower price.
With the MPXM2053GS I measure pressure from 10 to 180 Kpa (after playing with the offset and gain of the opamp). I assume I can do more or less the same with the MPX2300.
According to the datasheet of the MPXM2053GS it can handle 200Kpa, so fa so good. the datasheet of MPX2300 say it can handle 125 PSI.
Best regards,
Mike