MPR121 proximity capacitive sensor ic alternative

cancel
Showing results for 
Search instead for 
Did you mean: 

MPR121 proximity capacitive sensor ic alternative

1,302 Views
Contributor I

Hello,

I'm looking for a 16channel version of MPR121 ic. Searched a lot. But couldn't find any.

Proximity Capacitive Touch Sensor Controller|Freescale

Thanks.

Labels (2)
0 Kudos
1 Reply

80 Views
NXP Employee
NXP Employee

Hello Sreedev,

In this case, the MPR121 counts with 12 electrodes/capacitance sensing inputs in which 8 are multifunctional for LED driving and GPIO. The device also features a 13th simulated electrode which represents the simultaneous charging of all the electrodes connected together.

I am afraid there is not 16 channel version.

However, When the number of keys exceed the available sensor channels, multiplexing or logical combinations can be created.

In order to get more information, please refer to the AN3863​ especially at chapter 4.1.2.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos