MPL3115A2 alternative address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPL3115A2 alternative address

1,239 Views
szymondanilo
Contributor I

Hi all,

At the outset, I would like to apologize for the language mistakes in this email, because my English is basic.

I am writing on the barometric pressure MPL3115A2. In my project in which it is to be used needs to 2 such sensors were connected bus I2C. According to the datasheet, MPL3115A2 has a permanent address what prevents such connection.

I found the note also provides information to contact to find out the MPL3115A2 with an alternative address.

Do you have a state in the stock this sensors of the alternative addresses?

​Thanks.

​PS. I am a student and the project is created within the student research group. If you can get it as a sample?

Labels (1)
1 Reply

1,044 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Szymon,

You are right, unfortunately the MPL3115A2 does not have address select pins, so the fixed 7-bit slave address is 0x60. For small quantities, we recommend using an I2C multiplexer such as the PCA9544A.

You can order free samples of the MPL3115A2 with the slave address of 0x60 by clicking on the “Exlusive Sample” button on this website.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply