MPL3115 altitude accuracy over temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPL3115 altitude accuracy over temperature

439 Views
sreeharsha_anga
Contributor I

Hi,

I'm planning to use the MPL3115A2 in a low temperature environment(-20~30 degrees C) and wanted to know the accuracy of the altimeter under such conditions. Is the 0.3m accuracy still valid? Any caveats I should be aware of?

Labels (1)
0 Kudos
1 Reply

373 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sree,

Please distinguish between accuracy and resolution.

0.3m is resolution the MPL3115A2 can achieve when using maximum oversampling (OS[2:0] = 0b111). This is valid over the whole operating temp range.

However, accuracy will likely be worse than the one specified in the datasheet (±0.4kPa). 

Best regards,

Tomas

0 Kudos