MPL115A1 reflow environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPL115A1 reflow environment

850 Views
randywaite
Contributor I

We are using the MPL115A1.  The data sheet recommends reflow in an inert environment.  Is that to minimize corrosion of the part leads and board pads during reflow or is there a possibility of damaging the sensor itself?

0 Kudos
Reply
1 Reply

667 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Randy,

I am not entirely sure the context of the note in the data sheet since the author did not specify but it makes sense that during the reflow process, device pins to PCB contact pads are subject to oxidation when the boards are soldered in a standard air environment which can result in soldering defects. These soldering defects can be minimized if an inert gas such as nitrogen is used during the reflow process.

Regards,

Tomas

0 Kudos
Reply