MP3V5010DP with P1 < P2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MP3V5010DP with P1 < P2

1,303 Views
torkomairware
Contributor I

Would I damage the MP3V5010DP if I run it over a range of 50 kPa to 106 kPa at sea level?  In the range from 101 kPa to 106 kPa, P1 < P2. I am not tying to make measurements from 101 to 106 kPa, I just want to avoid damaging the sensor.

Labels (1)
0 Kudos
Reply
1 Reply

1,110 Views
miguelsalhuana
NXP Employee
NXP Employee

I would like to know some more details of your particular use case. Are you using this sensor as a gauged device (one port vented to atmospheric pressure)? When you say that you will be taking measurements at 101 to 106kPa is this atmospheric pressure or line pressure?

Regards,

Miguel

0 Kudos
Reply