MP3V5010DP with P1 < P2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MP3V5010DP with P1 < P2

666件の閲覧回数
torkomairware
Contributor I

Would I damage the MP3V5010DP if I run it over a range of 50 kPa to 106 kPa at sea level?  In the range from 101 kPa to 106 kPa, P1 < P2. I am not tying to make measurements from 101 to 106 kPa, I just want to avoid damaging the sensor.

ラベル(1)
0 件の賞賛
1 返信

473件の閲覧回数
miguelsalhuana
NXP Employee
NXP Employee

I would like to know some more details of your particular use case. Are you using this sensor as a gauged device (one port vented to atmospheric pressure)? When you say that you will be taking measurements at 101 to 106kPa is this atmospheric pressure or line pressure?

Regards,

Miguel

0 件の賞賛