I need help on Datasheet MP3V5004G Rev 2, 06/2010. There are pinouts (Style 1 and 2) indicated on each of pages 8 and 11, but nowhere is there anything to indicate which one applies where.
Solved! Go to Solution.
Hello,
Thank you for using the NXP community.
You are correct, in this case, the STYLE 2 is useful for the differential sensors.
Please note that a differential pressure sensors are used when the application calls for measuring the difference between two pressure points. One side of the sensor is hooked up to one pressure point, and the other side is hooked up to a different pressure point.
Thank you very much for your comments. I received your feedback and it was forwarded to the corresponding team.
Regards,
David
I'm looking at MP3V5004GP, DP and GVP.
Hello,
The STYLE 2 will be useful for you for GP and GVP, while the STYLE 1 for the DP.
Regards,
David
Hello,
Thank you for using the NXP community.
You are correct, in this case, the STYLE 2 is useful for the differential sensors.
Please note that a differential pressure sensors are used when the application calls for measuring the difference between two pressure points. One side of the sensor is hooked up to one pressure point, and the other side is hooked up to a different pressure point.
Thank you very much for your comments. I received your feedback and it was forwarded to the corresponding team.
Regards,
David
Hello RPAlex,
I hope all is great with you. Thank you for using the NXP communities.
Could you please let me know the exact part number used?
If you are using the MP3V5004DP for example (differential), then the STYLE 1 will be useful for you.
If you are not using the differential device option, then the STYLE 2 is the correct option for you.
I hope this information helps.
Regards,
David