Hi All,
Curently I am working on STM32L4RCT MCU and on MMA9553L connected to IIC. Is there any sample source code available for the same ?
Regards,
Prasanna
解決済! 解決策の投稿を見る。
The issue is monitored in different thread. Thank you for your info.Marking this question resolved.
https://community.freescale.com/message/621622?et=watches.email.thread#621622
Hi Prasanna,
As you also entered a similar thread in the ISF community forum (MMA955L pedometer issue in reading 6axis data), do you still need we provide you more inputs on this one ?
Regards, Jacques.
The issue is monitored in different thread. Thank you for your info.Marking this question resolved.
https://community.freescale.com/message/621622?et=watches.email.thread#621622
Hello Prasanna,
Unfortunately I do not have sample code for the MMA9553L device.
In this case, you may refer to the MMA9553L Intelligent Pedometer Platform Software Reference Manual.
This reference manual describes the features, architecture, usage examples, and programming model of the MMA9553L intelligent pedometer platform.
Please let me know if this information is useful for you.
If I misunderstood your question, feel free to let me know. I will be glad to help.
Have a great day.
David Diaz.
Note: If this post answers your question, please click the Correct Answer button. Thank you!
Thank you David for your quick response. I did send 0x00 0x00 0x00 0x0c to MMA9555L and receiving proper versions from it. But on sending 0x12 0x20 0x06 0x01 0x00 I am not receiving any valid data and instead receiving 0x00 0x80 0x0c 0x0c 0x7a 0xed as responce from it instead of receiving Accelerometer data. Also tried sending
0x04, 0x20, 0x2C, 0x0C, 0x06, 0x18, 0x06, 0x19, 0x06, 0x1A, 0x06, 0x1B, 0x06, 0x1C, 0x06, 0x1D then 0x18, 0x20, 0x00, 0x01, 0x10 and then reading 6 bytes of data,resulted in
0x00 0x80 0x0c 0x0c 0x20 0x2c
Can you please suggest the commands I am sending is wrong to get accelerometer data? Or is that I should send any other commands to receive valid accelerometer data from MMA9555L chip?
Regards,
Prasanna
Hello Prasanna,
I am glad to help.
Please be aware that the device powers up in Sleep mode, but it may become necessary to wake the part. This process uses the following mailboxes:
Once the device is awake, you may proceed with the pedometer application configuration as follow:
You may read the status registers properly.
Please let me know if this information is useful for you.
Have a great day.
David
Also for the commands you shared, Post sending
aTxBuffer[0] = 0x15;
aTxBuffer[1] = 0x20;
aTxBuffer[2] = 0x00;
aTxBuffer[3] = 0x10;
aTxBuffer[4] = 0x00;
aTxBuffer[5] = 0x10;
aTxBuffer[6] = 0x00;
aTxBuffer[7] = 0x10;
aTxBuffer[8] = 0x00;
aTxBuffer[9] = 0x00;
aTxBuffer[10] = 0x00;
aTxBuffer[11] = 0x00;
aTxBuffer[12] = 0x00;
aTxBuffer[13] = 0x00;
aTxBuffer[14] = 0x00;
aTxBuffer[15] = 0x00;
aTxBuffer[16] = 0x00;
aTxBuffer[17] = 0x06;
aTxBuffer[18] = 0x00;
aTxBuffer[19] = 0x10;
MMA955L_AcclDataTx(aTxBuffer, 20,0x15); //Send 20 bytes command to configure pedometer
//read status reg:
aTxBuffer[0] = 0x15;
aTxBuffer[1] = 0x30;
aTxBuffer[2] = 0x00;
aTxBuffer[3] = 0x0c;
and reading 16 bytes of data response I am receiving is 0x15, 0x30 ,0x0 ,0xc, 0x0 ,0x10,0x0,0x10,0x00,0x00,0x00,0x00,0x80,0xc,0xc,0x7a
Is that valid? As per data sheet 2 byte should be 0x80 but I am receiving 0x30. Is something wrong in sending ?
Regards,
Prasanna
Thank you David for your quick response. I did awake the device from sleep. I am in need only to read accelerometer data i.e x,y,z axis values and not speed etc. To achieve the same too should we send 0x15,0x20,0x0,0x10....... etc command??? As per data sheet to read accel data, I need to configure it as
aTxBuffer[0] = 0x1A;
aTxBuffer[1] = 0x20;
aTxBuffer[2] = 0x00;
aTxBuffer[3] = 0x02;
aTxBuffer[4] = 0x06;
aTxBuffer[5] = 0x10;
MMA955L_AcclDataTx(aTxBuffer, 6,0x1A); //Send i2c command to app ID 1A
aTxBuffer[0] = 0x1A;
aTxBuffer[1] = 0x10;
aTxBuffer[2] = 0x00;
aTxBuffer[3] = 0x02;
MMA955L_AcclDataTx(aTxBuffer, 4,0x1A);//Send i2c command to app ID 1A
memset(aRxBuffer, 0x00, sizeof(aRxBuffer));
MMA955L_AcclDataRx(aRxBuffer, 6,0x1A);
//Read status reg:
aTxBuffer[0] = 0x1A;
aTxBuffer[1] = 0x30;
aTxBuffer[2] = 0x00;
aTxBuffer[3] = 0x02;
MMA955L_AcclDataTx(aTxBuffer, 4,0x1A);// read request to acclerometer
if(COCO_BIT_Set)
MMA955L_AcclDataRx(aRxBuffer, 6,0x1A); //Read i2c data from 1A reg
Is this commands enough to read the accelerometer data?
Regards,
Prasanna