MMA8652fc tap detection without INT pins?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMA8652fc tap detection without INT pins?

1,290 次查看
villesavolainen
Contributor I

I am designing a board  with MMA8562fc and MSP430g2553 and the board should detect a double tap in z axis and turn on a LED when it happens. I didn't connect the INT pins, so i cannot use them. Does the tap detection feature work without these pins? Is it possible to read some register to check if the double tap has happened??

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,189 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ville,

Yes, there is the DPE bit in the PULSE_SRC register (0x22) that will be set when a double tap event is detected.

Best regards,

Tomas

0 项奖励
回复