MMA8652fc tap detection without INT pins?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8652fc tap detection without INT pins?

1,325 Views
villesavolainen
Contributor I

I am designing a board  with MMA8562fc and MSP430g2553 and the board should detect a double tap in z axis and turn on a LED when it happens. I didn't connect the INT pins, so i cannot use them. Does the tap detection feature work without these pins? Is it possible to read some register to check if the double tap has happened??

Labels (1)
0 Kudos
Reply
1 Reply

1,224 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ville,

Yes, there is the DPE bit in the PULSE_SRC register (0x22) that will be set when a double tap event is detected.

Best regards,

Tomas

0 Kudos
Reply