MMA8652 affected by sound vibration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8652 affected by sound vibration

612 Views
edmon
Contributor II

Hi, I am using MMA8652 in my project which also have Audio/Speaker. The speaker's vibration is affecting the data of the 3D accelerometer. At some point the vibration is considered as a TAP. Do you have any recommendation on how to mount MMA8652 or the speaker to avoid affecting my data. Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

400 Views
david_diaz
NXP Employee
NXP Employee

Hello Edmon,

In this case I recommend moving the pulse threshold value in order to avoid the undesired TAPs.

In order to change the threshold value, you may refer to the PULSE_THSX/Y/Z register.

TAP.jpg

In order to get detailed information about the TAP detection, you may refer to the Application Note AN3919​.

Beside, you may find sample code here.

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply