MMA8652 : Transient interrupt threshold value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMA8652 : Transient interrupt threshold value

1,750 次查看
koichisakagami
Contributor II

Dear community,

I consider the Transient interrupt threshold value.

In the case of setting to register value as follows,
when does the Transient interrupt occur ?

       0x1F:TRANSIENT_THS Register THS[6:0] to 000_0000b.
       0x1D:TRANSIENT_CFG Register HPF_BYP to  1.

Which is the Transient interrupt trigger point value ,
" greater than or equal to ZERO G " or " greater than ZERO G " ?

       Best Regards,
       Koichi Sakagami

标签 (1)
0 项奖励
回复
3 回复数

1,432 次查看
koichisakagami
Contributor II

Dear Tomas san,
Thank you for your reply.

> What is the use of such settings?
I would like to detect a less than 0.063g transient.

Best Regards,
Koichi Sakagami

0 项奖励
回复

1,432 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Koichi-san,

The minimum threshold resolution is 0.063g (TRANSIENT_THS = 0x01). None of our accelerometers offer higher resolution.

Best regards,

Tomas

0 项奖励
回复

1,432 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Koichi-san,

What is the use of such settings? The interrupt would be generated whenever the acceleration is higher than 0g.

Best regards,

Tomas

0 项奖励
回复