MMA8652 : Absolute maximum rating for Supply voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8652 : Absolute maximum rating for Supply voltage

Jump to solution
911 Views
koichisakagami
Contributor II

Dear community,

I consider the Supply voltage (VDD) specification .

In Table2. Maximum ratings of DataSheet Rev3.3,
the supply voltage maximum value is 3.6v .

Meanwhile, in Table5. Electrical characteristics,
the supply voltage maximum value is 3.6v .

[Question]
        Why are two parameters the same value ?

        I believe that the Absolute maximum rating is more bigger .

Best Regards,
       Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
701 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Koichi-san,

The TSMC specification indicates a max voltage of 3.6V and this was used for max operating and absolute max specs. We cannot put a higher value than our supplier puts. Also other customers have asked in the past what happens if small variations in power supply take the voltage above 3.6V slightly or in transient fashion. The MMA8652FC should certainly survive this but we cannot ever guarantee this in writing because TSMC does not, or may have special conditions on this.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

View solution in original post

0 Kudos
Reply
1 Reply
702 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Koichi-san,

The TSMC specification indicates a max voltage of 3.6V and this was used for max operating and absolute max specs. We cannot put a higher value than our supplier puts. Also other customers have asked in the past what happens if small variations in power supply take the voltage above 3.6V slightly or in transient fashion. The MMA8652FC should certainly survive this but we cannot ever guarantee this in writing because TSMC does not, or may have special conditions on this.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply