MMA8452Q, does not work with arduino Zero

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMA8452Q, does not work with arduino Zero

1,054 次查看
andrespinzon
Contributor I

Hy
I have a MMA8452Q sensor, I can configure with an Arduino UNO but when I try to control with arduino Zero does not work, I'm using the library Wire.h. When I ask arduino UNO with the register (WHO AM I)  respond as address 0x2A me, but when I ask register with the arduino Zero's feedback, this is 0x00.
What I can do to control the sensor with arduino Zero?

Thanks any help

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

907 次查看
anthonyduhamel
NXP Employee
NXP Employee

Hello Andres,

We can't really help you with your arduino boards. It looks to be a Mcu issue,probably with the wire.h (=I²C) library which may not work in the same way on the arduino zero.  I suggest to check the I²C frames with a logic analyser to compare the differences between the two devices.

Anthony

0 项奖励
回复