MMA8451Q starts transmitting zeros after the x-axis goes positive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8451Q starts transmitting zeros after the x-axis goes positive

Jump to solution
1,978 Views
petecotton
Contributor II

Hi,

We are using the MMA8451Q accelerometer in a project using i2c to communicate with an HCS08 processor. The x, y and z output values are transmitted fine as long as the x axis is a negative g number. We can tilt the board so the other two axis' go negative or positive and the data is still transmitted fine. The moment we tilt the board so that the x-axis goes positive the board starts transmitting 0,0,0 (0 on all three axis). Even if we move the board back so that the x-axis is negative again the board continues to broadcast 0,0,0 and will not resume normal operation until we power it off and back on again.

I have tried four separate chips and they all exhibit the same behaviour. Am I missing something fundamental here? Thanks in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,819 Views
petecotton
Contributor II

I finally discovered what the problem was.

My code was sending an acknowledge to the accelerometer after every read, including the last (7th) read. I should have sent a Not Acknowledge (i.e. nothing) after the last read. I have no idea why it exhibited itself in this weird x-axis behaviour - but it definitely fixed it (and removing the line reverts back to the broken behaviour.).

The missing line was
IICC_TXAK = 1;

Which suppresses the acknowledge bit on the next read.

Thanks for taking the time to look into it and for the advice.

Pete

See code below:

// Read FMode Register followed by the X MSB, XLSB, YMSB, YLSB, ZMSB and ZLSB registers (7 in total)

  IICC_TX=0;

  IICC_TXAK=0;

  IICD; // Generate clock pulses

  delay(6);

  accFMode = iic_ReadNextByteOffBus();

  accXmsb = iic_ReadNextByteOffBus(); // Read X Most Significant Byte (MSB)

  accXlsb = iic_ReadNextByteOffBus(); // Read X Least Significant Byte (LSB)

  accYmsb = iic_ReadNextByteOffBus(); // Read Y MSB Byte

  accYlsb = iic_ReadNextByteOffBus(); // Read Y LSB Byte

  accZmsb = iic_ReadNextByteOffBus(); // Read Z MSB Byte

  IICC_TXAK=1; // Don't send an acknowledge bit so that the accelerometer knows this is the last byte

  accZlsb = iic_ReadNextByteOffBus(); // Read Z LSB Byte

View solution in original post

0 Kudos
Reply
4 Replies
1,820 Views
petecotton
Contributor II

I finally discovered what the problem was.

My code was sending an acknowledge to the accelerometer after every read, including the last (7th) read. I should have sent a Not Acknowledge (i.e. nothing) after the last read. I have no idea why it exhibited itself in this weird x-axis behaviour - but it definitely fixed it (and removing the line reverts back to the broken behaviour.).

The missing line was
IICC_TXAK = 1;

Which suppresses the acknowledge bit on the next read.

Thanks for taking the time to look into it and for the advice.

Pete

See code below:

// Read FMode Register followed by the X MSB, XLSB, YMSB, YLSB, ZMSB and ZLSB registers (7 in total)

  IICC_TX=0;

  IICC_TXAK=0;

  IICD; // Generate clock pulses

  delay(6);

  accFMode = iic_ReadNextByteOffBus();

  accXmsb = iic_ReadNextByteOffBus(); // Read X Most Significant Byte (MSB)

  accXlsb = iic_ReadNextByteOffBus(); // Read X Least Significant Byte (LSB)

  accYmsb = iic_ReadNextByteOffBus(); // Read Y MSB Byte

  accYlsb = iic_ReadNextByteOffBus(); // Read Y LSB Byte

  accZmsb = iic_ReadNextByteOffBus(); // Read Z MSB Byte

  IICC_TXAK=1; // Don't send an acknowledge bit so that the accelerometer knows this is the last byte

  accZlsb = iic_ReadNextByteOffBus(); // Read Z LSB Byte

0 Kudos
Reply
1,819 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Pete,

I have never heard of a similar problem. If you have a logic analyzer or an oscilloscope, could you please share here an image illustrating what is going on the bus? Are you able to read the WHO_AM_I register when the X axis goes positive?

Regards,

Tomas

1,819 Views
petecotton
Contributor II

Thank you Tomas for your quick response. I can confirm that I can read the WHO_AM_I register correctly when the X axis is negative, but as soon as the X axis goes positive the WHO_AM_I register also starts to return 0. Moving the x-axis back negative again does not fix the issue and it continues to read 0 for WHO_AM_I until I do a power off/on on the board.

Unfortunately the components on the printed circuit board (a prototype board) are too small to solder on to or get probes on to, however I have ordered the individual components and will try and replicate the processor-accelerometer part of the circuit on a breadboard. Then I will be able to get the logic analyser on it and I will post a picture of what's happening on the bus.
At least now I know I'm not just missing something obvious :-)

Thank you again. I will probably have the circuit built early next week and will post then.

0 Kudos
Reply
1,819 Views
petecotton
Contributor II

Update: I just noticed something when applying your test. If I do not read the x,y,z registers (0x00 to 0x06), then I can still read the WHO_AM_I register, even when the x axis is positive. The moment I read the x,y,z registers (with x positive), then all other registers return 0. So, the problem only appears when I try to read the x,y,z registers when x is positive.

0 Kudos
Reply