MMA8451Q - Single and double-tap detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8451Q - Single and double-tap detection

Jump to solution
981 Views
terryj
Contributor I

Hello,

I would like to detect a single-tap and double-tap by interrupt signals.

Is the following interrupt setting possible?


Single tap detect -> INT1

Double tap detect -> INT2


Thank you,

Terry

0 Kudos
Reply
1 Solution
666 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Terry,

It is not possible. You can detect either a single pulse or a double pulse, but not on separate interrupt pins.

Regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
667 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Terry,

It is not possible. You can detect either a single pulse or a double pulse, but not on separate interrupt pins.

Regards,

Tomas

0 Kudos
Reply