MMA8451Q Accelerometer I2C Sink Current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMA8451Q Accelerometer I2C Sink Current

3,124件の閲覧回数
ian1322
Contributor I

Does anyone know what the maximum sink current for the I2C interface is for this part?  That is, what’s the maximum allowable IOL for SDA or SCL ?  I realize the I2C spec lists these as 3 mA (400 kHz) and 20 mA (1 MHz), but it seems this isn't a hard requirement because many datasheets list other values for these (effectively limiting the maximum bus capacitance). 

ラベル(1)
1 返信

2,676件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ian,

Attached you can find current capability characteristics of both SCL and SDA pads.

Please note that the MMA8451Q is compliant with NXP I2C specification for both Standard and Fast modes only (400 kHz max).

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信