MMA6827

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMA6827

2,175 次查看
Zhang_123
Contributor II

I would like to ask how the sensitivity of the MMA6827 is calculated, and why the sensitivity of the 120g 10bit data bit is 0.24414  Thank you very much

0 项奖励
回复
6 回复数

2,156 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

First, please note that this device is obsolete. Let me know if you need a further recommendation for a replacement device.

The sensitivity of the device is mentioned on the chapter 3.4 from the datasheet:

diazmarin09_0-1679437649676.png

 

No additional calculation is needed, just the signed decimal value from the 10-bit digital output multiplied by the sensitivity (g/LSB) and you get the acceleration in Gs. Note that the acceleration is given in LSB/g so you need to calculate the reciprocal.

Example: reciprocal(4.096 LSB/g) x 480 LSB  =  117.19 g   (trimmed for maximum range)

 

I hope this information helps.

Regards,

David

0 项奖励
回复

2,037 次查看
Zhang_123
Contributor II

Thank you so much!

0 项奖励
回复

2,152 次查看
Zhang_123
Contributor II

Thank you very much for your answer,

Zhang_123_0-1679443947587.png

I would like to know how the sensitivity of 0.24414 is calculated based on the range in the table above, thank you very much!

0 项奖励
回复

2,145 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

Thank you for using the NXP community.

In that case, those values are related to the thresholds to be used by the arming function. Refer to Section 4.8.9 at datasheet for more details regarding the arming function.

 

I hope this information helps.

Regards,

David

0 项奖励
回复

2,136 次查看
Zhang_123
Contributor II

Thank you very much for your previous answer. I wonder if the MM6827 can set the range and sensitivity? I didn't see the specific register, thank you very much!

标记 (1)
0 项奖励
回复

2,133 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

Thank you for reaching out to us.

I am afraid that both the range and sensitivity are fixed.

diazmarin09_0-1679593253554.png

 

Please let me know if you need a further recommendation for a replacement device.

Regards,

David

0 项奖励
回复