MMA51XX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA51XX

584 Views
Jhonemagee
Contributor I

Can this sensor be connected directly to the psi5 port of the ecu

0 Kudos
Reply
6 Replies

566 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jhonemagee,

if your ECU has the PSI5 1.3 version, then yes. 

JozefKozon_0-1706604647383.pngJozefKozon_1-1706604679830.png

Alternatively you can use our SEN-PSI5-ADAPTER

https://www.nxp.com/docs/en/user-guide/UM11524.pdf

With Best Regards,

Jozef

0 Kudos
Reply

557 Views
Jhonemagee
Contributor I

Dear JozefKozon,

Is the No. 3 pin IDATA of the chip output a current signal or a voltage signal?

0 Kudos
Reply

519 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jhonemagee,

please refer to the section 4.2.1.2 in the MMA51xxKW datasheet. The IDATA pin sources current. So it is a current pin. 

JozefKozon_2-1706854937915.png

JozefKozon_3-1706854985461.png

 

With Best Regards,

Jozef

0 Kudos
Reply

558 Views
Jhonemagee
Contributor I

Dear JozefKozon,

We ECU has the PSI5 1.3 version.  I wonder if this sensor can directly implement synchronous parallel mode without PHY. Just like the picture says

微信图片_20240131084618.jpg

 

0 Kudos
Reply

548 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jhonemagee,

the recommended connection for the MMA51xx sensors is daisy chain as in the Figure 25. in the MMA51xxKW datasheet. It is similar to your bus configuration with added discrete components. The recommended external components are in the Table below the Figure 1. 

JozefKozon_4-1706680777068.png

Screenshot_1.png

JozefKozon_3-1706680488513.png

Please also refer to this document, where an application example for PSI5-P10P-500/3L compatible sensors is described.  

JozefKozon_2-1706680456729.png

With Best Regards,

Jozef

0 Kudos
Reply

530 Views
Jhonemagee
Contributor I

Dear JozefKozon,

Is the No. 3 pin IDATA of the sensor output a current signal or a voltage signal?

0 Kudos
Reply