MC33774均衡最多可打开通道数

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33774均衡最多可打开通道数

329 Views
Sally_Wang
Contributor I

您好,

想请教一下,MC33771这个芯片对均衡是否有限制,配置的每个通道独立打开均衡开关,均衡单个可以打开,但是想14个通道全部打开时,不能控制,打开到第6点均衡,就不可以了,手册上提供的数据是均衡限制电流为300mA,两个MC33771的芯片采集28 或者小于28串的电压值,都是只能打开到第六节,测量出单节打开的均衡电流大约在80mA,请问下这个是IC决定还是通过软件寄存器配置可修改该参数。

0 Kudos
Reply
2 Replies

311 Views
guoweisun
NXP TechSupport
NXP TechSupport

应该都是可以打开的您看下datasheet page50-7.5.4 Cell balancing process

里面有详细的操作步骤 MC33774

Tags (1)
0 Kudos
Reply

282 Views
Sally_Wang
Contributor I
弄错了,是MC33771,实际电路控制没有问题,配置了独立控制,但是不能所有通道同时打开,手册上写的是可以同时打开的,最大的均衡电流额300,请问这个参数是否可配置,可修改,如何实现所有通道均衡都打开。
0 Kudos
Reply