MC33771C OC Fault detection speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33771C OC Fault detection speed

1,071 Views
JuanDavid
Contributor I

Hello,

I'm running tests with this BCC and in the case of the OC detection the timing I see from the datasheet is different from what I'm getting.

I'm reading around 300uS from the current reaching the OC limit to the Fault Pin being UP.

ADC resolution is 16 bit.

BCC is in continuous measurement mode.

According to the datasheet the time it takes for ADC2 to perform the current reading is 40uS.

What am I missing?

Thank you.

0 Kudos
Reply
2 Replies

1,058 Views
JuanDavid
Contributor I

Thank you Tomas.

As you pointe out probably the delay is cause by my filter which is the same recommended in the datasheet..

Also I'd like to ask about that parameter from the datasheet. It specifies that those 56us happen in normal mode but the overcurrent fault happens ONLY in sleep mode. Does tfault varies in that case?

Thank you.

0 Kudos
Reply

1,064 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Juan,

 

What is the filter that you have on the current sense line? What is its time constant?

Could you please share a scope plot illustrating your measurements?

As shown in the datasheet, the fault pin should be activated within 56us from the fault event.

Tfault.JPG

 

Best regards,

Tomas