MAG3110 calibration of devices that don't move

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAG3110 calibration of devices that don't move

4,728 Views
michaelcallahan
Contributor I

I have a device that doesn't move after being turned on but I would like to know which direction it is facing.  The MAG3110 magnetometer calibration instructions involve moving devices around (figure 8 or similar) to fit a solution to the resulting range of measurements.  How reasonable is it to assume that I could determine the hard and soft iron calibration for a small sample of PCBs/devices and use it for all others with the same layout?

Labels (1)
Tags (2)
0 Kudos
Reply
7 Replies

3,683 Views
172809727
Contributor I

Hi.

   i use the calibration way refer to the demo. But i don`t know why this way can calibration, if i am wrong. how i can use mag3110 enbedded offset?

   the screenshot is my calibration way

捕获.PNG

0 Kudos
Reply

3,683 Views
anthonyduhamel
NXP Employee
NXP Employee

Hello Mandy,

This software function is supposed to calibrate the HardIron (offset brought by the board and the magnetometer). But this will work with one essential condition : you need to rotate the board/MAG31110 over the 3-axis during the execution of the calibration !

Look at the chart below (here, the board rotates at a constant speed, but you don't need to do that)

pastedImage_1.png

By rotating the magnetometer, you will change the magnetic field (induced by the Earth, like a compass). By capturing the min and max values, you will by able to calculate the offset of the MAG3110. By writing theses values in the OFF_axis_xSB register, the MAG3110 will be able to apply this hardiron vector compensation to the raw measurements: that's the calibration.

Hope this helps you,

Anthony

0 Kudos
Reply

3,683 Views
172809727
Contributor I

if i just want to know the angle between to the horizontal. how can i do with mag3110? need i calibrate? please tell me how to do detailed

发自我的iPhone

0 Kudos
Reply

3,683 Views
anthonyduhamel
NXP Employee
NXP Employee

Yes you need to calibrate. If you don't, you will have inacurrate results.

pastedImage_1.png

0 Kudos
Reply

3,683 Views
172809727
Contributor I

if i just want to calculate the angle between the horizontal how can i do?

发自我的iPhone

0 Kudos
Reply

3,683 Views
anthonyduhamel
NXP Employee
NXP Employee

Please check the Tomas' response. 

how to deal the data from mag3110 

With the additional information I give to you, you should be able to understand how to do it : use the hardiron calibration, then apply arctan(Y/Z). You have all the pieces, you just need to merge it altogether.

Anthony

0 Kudos
Reply

3,683 Views
anthonyduhamel
NXP Employee
NXP Employee

Hello Ben,

Did you use the MAG3110 embedded offset calibration or a real magnetic external calibration? If it is the auto-calibration, it's going to work on 1,2 or 3 axis.

It's hard to say how reasonable is it to perform a "static(non dynamic) calibration" I would say no, but it depends on your final application. Can you tell us more about it?

Thank you,

Anthony

0 Kudos
Reply