MAG3110 Temperature Sensitivity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MAG3110 Temperature Sensitivity

830 次查看
gdg
Contributor I

I am seeing magnetometer readings change by ~0.5 uT/degC (in each axis) when reading earth fields of about 30 uT.  This seems much larger than the specified sensitivity change due to temperature (0.1%) for this device, since 0.1% of 30 uT is 0.03 uT.  This is the case for multiple units.  Is this expected performance, and if not is there anything else I should be checking?

标记 (1)
0 项奖励
回复
0 回复数