Low Pass Filter Question. (SensorFusion Library 7.0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Low Pass Filter Question. (SensorFusion Library 7.0)

跳至解决方案
1,023 次查看
youngguekim
Contributor III

Hi. 

I want to use a only accelerometer. So I am using a Function : "fRun_3DOF_G_BASIC"

 

My Question is :

fRun_3DOF_G_BASIC has a LPF Function "fLPFOrientationQuaternion"

and the rotation matrix should convert into Quaternion for Low pass filter.

 

is it impossible that Rotation matrix has Low pass filter directly without converting Quaternion??

Why they go through the step 1, 3   bearing the loss of time

 

 

step 1 : fQuaternionFromRotationMatrix

step 2 : fLPFOrientationQuaternion

step 3 : fRotationMatrixFromQuaternion

step 4 : fNEDAnglesDegFromRotationMatrix

标签 (1)
0 项奖励
1 解答
774 次查看
michaelestanley
NXP Employee
NXP Employee

We've not found a method we are comfortable with to low pass filter a rotation matrix directly.  Quaternions are simpler and have some very nice properties numerically.  So yes, this is the way we chose to go.  FYI, none of these operations takes a lot of time to execute.  You should be using a small fraction of your available CPU cycles.

Regards,

Mike

在原帖中查看解决方案

2 回复数
775 次查看
michaelestanley
NXP Employee
NXP Employee

We've not found a method we are comfortable with to low pass filter a rotation matrix directly.  Quaternions are simpler and have some very nice properties numerically.  So yes, this is the way we chose to go.  FYI, none of these operations takes a lot of time to execute.  You should be using a small fraction of your available CPU cycles.

Regards,

Mike

774 次查看
youngguekim
Contributor III

Thank you for your kind reply

0 项奖励