Long term accuracy of the MP3V5004G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Long term accuracy of the MP3V5004G

1,099 Views
lassecrone
Contributor I

Hi

Are there any data on how/if the accuracy of the MP3V5004G can be expected to change over time?

Best regards

Lasse

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

983 Views
Joshevelle
Senior Contributor I

Hello Lasse,


The MP3V5004G is laser trimmed, but offset can shift due to temperature changes, mechanical stresses (mounting stresses) and aging. Since there tends to be an endless amount of various applications and conditions there has been no way Freescale can validate the application impact on product reliability or lifetime.

I would recommend you to take a look at AN1636 which describes how to implement an autozero function in order to correct the sensor output for longterm offset drift or variation.

http://cache.freescale.com/files/sensors/doc/app_note/AN1636.pdf

Hope it helps.

Josh

0 Kudos
Reply