LF signal reception on NTM88 TPMS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LF signal reception on NTM88 TPMS

1,143 次查看
nikita_kanade
Contributor I

Hello,

I am trying to receive the data on LF module in NTM88 TPMS.

Configured the LF module in Data reception mode

device wakeup Due to LF carrier and error flag is set

so unable to debug where is problem like in Premble or sync byte or in wakeup id or in data

Is any way to check received data on LF module like connecting any pin to DSO.

I used X-TPMS88EH11S434 board as LF receiver

and LF transmitter which send 2 ms preamble , 9 T pattern of sync pattern, 2 byte of wakeup id

Following are my LF module setting:

LFCTL1_LFEN = 0;

/* Wait 3ms before writing in the registers */
Delay_TPM_ms(3);

/* Low consumption during sniff mode + LF Ack */
LFS = (LFS_LPSM_MASK | LFS_LFIAK_MASK);

/* LFCTRLE to LFCTRLB are taken care of by vnfLFRConfigFactoryRegs called in TPMS_LF_ENABLE() */

LFCTRLA = 0;
LFCTRLB_LFPOL = 1;
LFCTL2 = 0;
LFCTL3 = (LFCTL3_T9_PATTERN | LFCTL3_DATA_1024_USEC_CARRIER_1024_USEC);

/* Enable Data Mode interrupts, enable the digital decoder and carrier */
/* validation, and set sync time-out */
LFCTL4 = (LFCTL4_LFDRIE_MASK | LFCTL4_DCEN_MASK | LFCTL4_VALEN_MASK
| LFCTL4_SYNC_SET_TO_24_MSEC | LFCTL4_LFCDIE_MASK | LFCTL4_LFIDIE_MASK);//|LFCTL4_LFERIE_MASK);

/* Set ID values */
LFIDH = ((UINT8) 0x12u);
LFIDL = ((UINT8)0x34u);

/* Disable carrier mode */
LFCTL1_CARMOD = 0;

/* Set ID type to 16-bit type */
LFCTL1_IDSEL = IDSEL_TYPE_16_BIT;

/* Set sensitivity */
LFCTL1_SENS = 2; // High sensitivity

 

0 项奖励
回复
1 回复

1,134 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Nikita,

the reason could be input saturation. Please refer to section  in AN4391. There is description of the fault and in section 4.2 is NXP recommendations how to solve it. The AN4391 can be downloaded from the NTM88 product page. There is lot of other documents to the NTM88 TPMS, which might interest you.

JozefKozon_0-1666257290413.png

With Best Regards,

Jozef

0 项奖励
回复