Hi,
I've just started using the Kinetis MCU series, and would like to take advantage of the sensor fusion library for motion tracking and gesture recognition.
Is the KL15 MCU series compatible with sensor fusion libraries?
It appears the evaluation version requires use of MQXLite, does the full development version require this too?
I wasn't planning on integrating MQXLite with the project, but if I were, is there an additional licensing cost associated with it?
Thanks,
Solved! Go to Solution.
Stephen,
If you haven't already, make sure you grab the latest sensor fusion release from http://www.freescale.com/sensorfusion. We no longer have separate evaluation and development versions. The kit now includes complete source code for all functions with no license checks at all. It's totally open (and free). You will need a KL15 variant with 128K flash/16K RAM. MQXLite it not required, but you will need to instrument high, medium and low priority tasks for sensor sampling, fusion and magnetic calibration respectively. This page has a discussion on portability topics.
Let me know if there are unanswered questions after you read it.
Mike
Stephen,
If you haven't already, make sure you grab the latest sensor fusion release from http://www.freescale.com/sensorfusion. We no longer have separate evaluation and development versions. The kit now includes complete source code for all functions with no license checks at all. It's totally open (and free). You will need a KL15 variant with 128K flash/16K RAM. MQXLite it not required, but you will need to instrument high, medium and low priority tasks for sensor sampling, fusion and magnetic calibration respectively. This page has a discussion on portability topics.
Let me know if there are unanswered questions after you read it.
Mike
Hi Michael,
Thanks for the info! Really happy to see that the project has been open-sourced.
Stephen