KIT912J637EVME TEMPLATE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KIT912J637EVME TEMPLATE

Jump to solution
1,523 Views
henriquekuehne
Contributor I

Hi,

I just bought the evaluation board KIT912J637EVME and the item CD912J637 referenced on User Manual http://www.nxp.com/assets/documents/data/en/user-guides/KT912J637UG.pdf  is not supplied anymore.

Could someone send me the template to project using the MM912J637 component for battery monitoring?

Thank you in advance,

Henrique.

Labels (1)
0 Kudos
Reply
1 Solution
1,147 Views
david_diaz
NXP Employee
NXP Employee

Hello Henrique,

Please review the file attached to this response. You may find the template requested.

 

I hope this material helps.

Regards,

David

View solution in original post

0 Kudos
Reply
3 Replies
1,146 Views
FlavioAlves
Contributor II

Hello,

Can we find the firmware implementation of the this presentation: http://cache.freescale.com/files/training/doc/dwf/DWF13_AMF_AUT_T1043.pdf ?

There is a project located at the following thread: https://community.nxp.com/thread/319590 . With this project it is possible to capture voltage, current and temperature. But it doesn't implement SOC algorithm, in the same way as presented.

Can you give us some guidelines about how to have this implementation?

Best regards,

Flavio

0 Kudos
Reply
1,146 Views
henriquekuehne
Contributor I

Hello David,

Thank you very much for your help.

This is what I was looking for.

Unfortunately, I thought that it would have an example of Coulomb Counter implemented, but it does not have.

Thank you again and best regards,

Henrique.

0 Kudos
Reply
1,148 Views
david_diaz
NXP Employee
NXP Employee

Hello Henrique,

Please review the file attached to this response. You may find the template requested.

 

I hope this material helps.

Regards,

David

0 Kudos
Reply