K22 Freedom board with intelligent Sensing Framework v2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K22 Freedom board with intelligent Sensing Framework v2.0

1,115 Views
marks
Contributor IV

Hi, I'm using the K22 Freedom board with the FRDM-STBC-AGM01. Everthing seems to work great. I am also using the Intelligent Sensing Framework v2.0 and following along with the  the traning videos. I discovered the "Kinetis Interface Tool" watching the 3rd video. So I downloaded it and tried to use it. However it will not reconize the board(s). The correct com port number shows up but I get a "No Compatible Device found at selected COM Port!" message. Is this hardware not supported?

 

Also, when is ISF 2.2 going to be released?

 

Thanks,

Mark

Labels (1)
0 Kudos
Reply
0 Replies