Issue with Coulomb count in BMS S32K144 Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with Coulomb count in BMS S32K144 Board

Jump to solution
1,528 Views
thailivenkatesh
Contributor III

Hi,
    using s3k144 Board want calculate the SOC for 6AH Battery .but i am getting Coulomb Count measurement result as 2136050216.
and calculated the I_AVG using the formula below.

#define BCC_GET_COULOMB_CNT(coulombCnt1, coulombCnt2) \
((int32_t)(((uint32_t)((coulombCnt1) & BCC_R_COULOMB_CNT_MSB_MASK) << 0xFU) | \
(((uint32_t)(coulombCnt2) & BCC_R_COULOMB_CNT_LSB_MASK)))

rawVal = (int32_t)BCC_GET_COULOMB_CNT(measurements[BCC_MSR_COULOMB_CNT1],
measurements[BCC_MSR_COULOMB_CNT2]);

I_AVG = (rawVal - COULOMB_CNT_old)/(measurements[BCC_MSR_CC_NB_SAMPLES] -CC_NB_SAMPLES_old); // this is average current
COULOMB_CNT_old = rawVal;
CC_NB_SAMPLES_old =measurements[BCC_MSR_CC_NB_SAMPLES];
or
I_AVG = rawVal/measurements[BCC_MSR_CC_NB_SAMPLES] ;

test results as follows

###############################################
| Cell 1 Voltage | 3322 mV |
| Cell 2 Voltage | 3322 mV |
| Cell 3 Voltage | 3322 mV |
| Cell 4 Voltage | 3347 mV |
| Cell 5 Voltage | 3286 mV |
| Cell 6 Voltage | 3314 mV |
| Cell 7 Voltage | 3323 mV |
| Cell 8 Voltage | 3315 mV |
| Cell 9 Voltage | 3317 mV |
| Cell 10 Voltage | 3317 mV |
| Cell 11 Voltage | 3317 mV |
| Cell 12 Voltage | 3122 mV |
| Coulomb Count | 2131001874|
| CC Samples | 31553 |
| I_AVG | 67537 |
| Current | -50 mA |
| StackVoltage | 39584 mV |
| Temperature | 25 degC |


###############################################


1. 6 Ah = 6*3600 = 21600 Coulombs = 100% SOC

2. So 1% SOC = 21600/100 = 216 Coulombs

But when i measure CC i am getting as 67537 coulombs for 6Ah battery unable to calculate the correct SOC.
Please support this issue to solve how to calculate exact values.

0 Kudos
1 Solution
1,427 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Venkatesh Thaili,

please refer to the section 9.7 in the MC33771C datasheet. Please check the FAULT pin in case the COULOMB_CNT overflow.

In the event an overflow occurs in either COULOMB_CNT or CC_NB_SAMPLES, the
CC_OVR_FLT bit is set and, when unmasked, the FAULT pin is activated. The coulomb
count value is impacted by conversions performed during diagnosis of the current
measurement chain.

The COULOMB_CNT is an integer whose associated resolution is V2RES, therefore,
COULOMB_CNT·V2RES gives μV. If the shunt resistance RSHUNT is expressed in μΩ,
then COULOMB_CNT·V2RES / RSHUNT gives μA.

With Best Regards,

Jozef

View solution in original post

1 Reply
1,428 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Venkatesh Thaili,

please refer to the section 9.7 in the MC33771C datasheet. Please check the FAULT pin in case the COULOMB_CNT overflow.

In the event an overflow occurs in either COULOMB_CNT or CC_NB_SAMPLES, the
CC_OVR_FLT bit is set and, when unmasked, the FAULT pin is activated. The coulomb
count value is impacted by conversions performed during diagnosis of the current
measurement chain.

The COULOMB_CNT is an integer whose associated resolution is V2RES, therefore,
COULOMB_CNT·V2RES gives μV. If the shunt resistance RSHUNT is expressed in μΩ,
then COULOMB_CNT·V2RES / RSHUNT gives μA.

With Best Regards,

Jozef