Is there any document about power cycling of a gyroscope of NXP? Specifically, i am interested in a current consumption profile (or model) for single sample method!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any document about power cycling of a gyroscope of NXP? Specifically, i am interested in a current consumption profile (or model) for single sample method!

854 次查看
giovannischibon
Contributor I

Ideally i would like to have a odcumentation like the one from paper "Achieving Lowest Power Consumption with MMA8491Q Accelerometer/Tilt Sensor".

0 项奖励
回复
1 回复

786 次查看
david_diaz
NXP Employee
NXP Employee

Hello Giovanni,

Unfortunately, there is no such document.

The FXAS21002C is a low power device. The current consumption in Active mode is 2.7 mA.

In this case, I would recommend to transit from Active to Ready mode when no measurements are being made. This mode offers the user the ability to significantly reduce the current draw of the device while providing a fast transition into Active mode within 1/ODR + 5ms.

I hope this information helps.

Regards,

David

0 项奖励
回复