Is there any difference between MPXV5004GC6T1, MPXV5004GC6U and MPVZ5004GC6U?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any difference between MPXV5004GC6T1, MPXV5004GC6U and MPVZ5004GC6U?

跳至解决方案
1,292 次查看
jasongao
Contributor I

I am looking for a diff air pressure sensor and find MPxx5004G is very suitable for our application.

After I read the datasheet, I find there are 3 different part numbers for case number 98ASB17757C.

So I want to ask is there any difference between these 3 part numbers?

Thanks a lot!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,105 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Jason,

Operationally speaking, these devices works the same way, but the only difference between the MPXV5004GC6T1 and the MPXV5004GC6U is the way they are shipped: MPXV5004GC6T1 is shipped in Reel, while the MPXV5004GC6U is shipped in Rail as stated in page 2 of the datasheet.

And the difference between these devices with the MPVZ5004GC6U is that the internal gel of this device is “Media Resistant gel” while in the other 2 devices use a fluorosilicone gel to isolates the die surface and wire bonds from the environment.

The Fluorosilicone Gel (Type FE-53) is being used for all our standard type of pressure sensors.

Media Resistant Gel (Sifel) is being used for our pressure sensors that are used e.g. in high temperature environments, mainly in automotive applications.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,106 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Jason,

Operationally speaking, these devices works the same way, but the only difference between the MPXV5004GC6T1 and the MPXV5004GC6U is the way they are shipped: MPXV5004GC6T1 is shipped in Reel, while the MPXV5004GC6U is shipped in Rail as stated in page 2 of the datasheet.

And the difference between these devices with the MPVZ5004GC6U is that the internal gel of this device is “Media Resistant gel” while in the other 2 devices use a fluorosilicone gel to isolates the die surface and wire bonds from the environment.

The Fluorosilicone Gel (Type FE-53) is being used for all our standard type of pressure sensors.

Media Resistant Gel (Sifel) is being used for our pressure sensors that are used e.g. in high temperature environments, mainly in automotive applications.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,105 次查看
jasongao
Contributor I

Hi Jose,

Thanks for your reply, it's very helpful for me, now I understand these. Thanks again.

Best regards,

Jason

0 项奖励
回复