Is there already a new ASIC revision available of the FXAS21002C?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there already a new ASIC revision available of the FXAS21002C?

1,127件の閲覧回数
johandejong
Contributor I

In a design, I used the FXAS21002C, which seems to have a problem with 4-wire multipoint SPI communication. In the errata (which I discovered when debugging the failing design) can be read that a new ASIC revision is planned for the first half of 2015. It is currently mid May 2016, so I wonder, is there already a new ASIC available? If yes, how do I find parts with the new date code?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

782件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hello,

Hi Johan,

I’ll contact the design team to check if the new ASIC is available, but I would need further details about your end product and application, can you please answer to the following questions, please?

  1. What are your end product(s) and the application?
    2.  When is your targeted production date or timeframe?
    3.  What is your projected volume/quantity?
    4.  Are you presently working with any of the following?
    (a) NXP/Freescale Semiconductor Representative
    (b) NXP/Freescale Semiconductor Distributor
    (c) Contract Manufacturing Representative

You can send me a private message if you do not want to make this information public.

I’m following you already, but in case you want to send me a private message, you would also need to “follow me” by clicking in “follow” in my profile.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信