INT0 for changes in x/y/z values and INT1 on vector magnitude.

cancel
Showing results for 
Search instead for 
Did you mean: 

INT0 for changes in x/y/z values and INT1 on vector magnitude.

Jump to solution
397 Views
intrudert
Contributor II

Is it possible to program FXOS7800cq this way : 

 1. INT0 will be generated when there's a chance in the magnetic x/y/z threshold values 

2. INT1 for magnetic vector change?

For example, my initial x/y/z values of magnetic sensor are set to 0/0/0 on start up. If  x or y or z value crosses 100, generate INT0.

My magnetic vector magnitude threshold is 80 uT. If it exceeds, generate INT1 .

Labels (2)
0 Kudos
1 Solution
118 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

Yes, it can be done.

1. Using the magnetic threshold event detection block. See chapter 14.16 of the FXOS8700CQ datasheet. The m_ths_int_cfg is used to select either INT1 or INT2.

2. Using the magnetic vector-magnitude change detection block. See chapter 14.18 of the FXOS8700CQ datasheet. The m_vecm_init_cfg bit is used to select either INT1 or INT2.

Hope it helps.

Best regards,

Tomas

View solution in original post

3 Replies
119 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

Yes, it can be done.

1. Using the magnetic threshold event detection block. See chapter 14.16 of the FXOS8700CQ datasheet. The m_ths_int_cfg is used to select either INT1 or INT2.

2. Using the magnetic vector-magnitude change detection block. See chapter 14.18 of the FXOS8700CQ datasheet. The m_vecm_init_cfg bit is used to select either INT1 or INT2.

Hope it helps.

Best regards,

Tomas

View solution in original post

118 Views
intrudert
Contributor II

What about directing both interrupts to the INT0 ?

0 Kudos
118 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

You can use the same INTx pin for both events. Then you will have to go to read the M_INT_SRC register (0x5E) to know which event caused the interrupt.

M_INT_SRC register.PNG

Best regards,

Tomas