I want to use MMA8451Q. Does Freescale.com offer the configuration file and some code examples?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to use MMA8451Q. Does Freescale.com offer the configuration file and some code examples?

1,172 Views
pukathy
Contributor I

I want to use MMA8451Q. Does Freescale.com offer the configuration file and some code examples?

Labels (1)
Tags (1)
1 Reply

980 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Try to look at my simple bare metal example project:

https://community.freescale.com/docs/DOC-98836

There are also several application notes describing embedded functions (e.g. orientation, motion, tap detection) including register settings:

http://www.freescale.com/products/sensors/accelerometers/3-axis-accelerometers/2g-4g-8g-low-g-14-bit...

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.