I want to detect the guesture based on the accelerometer and gyrometer values from imx7ulp board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I want to detect the guesture based on the accelerometer and gyrometer values from imx7ulp board

5,311件の閲覧回数
ravicalm
Contributor I

Hi Team,

Could you guys help me what kind of IMU sensor are u using in imx7ulp board to detect the accelerometer and gyrometer values. how we can predict the guestures with the gyrometer and accelerometer values.

 

Thanks and Regards,

Ravi

0 件の賞賛
返信
2 返答(返信)

5,291件の閲覧回数
ravicalm
Contributor I

Hi can u suggest a c programme which can do for detecting guesture if I have the data

0 件の賞賛
返信

5,294件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ravi,

As you can see in the attached schematic, to detect acceleration, you can use either the FXLS8952 or FXOS8700. To measure angular rate, you can use the FXAS21002.

Predicting reliably gestures using accelerometer/gyrometer data is not an easy task and typically involves applying machine learning algorithms to the sensors data.

BR, Tomas

0 件の賞賛
返信