I'm looking for the right processor for a MMA865...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm looking for the right processor for a MMA865...

1,031件の閲覧回数
christophergaud
Contributor I

Dear members,

i'm a newbie in this chat. But i hope you can help me. Our company is looking for the right processor for using an MMA865 accelerometer. We want to detect the deceleration and the tilt of a vehicle. It is necessary that  the detection is very fast and the current consumption as low as possible because we want to use Energy Harvesting. Thank you for your answers.

ラベル(1)
0 件の賞賛
返信
1 返信

695件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Christopher,

Several options for you and others probably have good advice too.

The Freedom boards for the Kinetis L Series of MCU's (KL02/KL03/KL05) are low power and have an accelerometer (MMA8451Q 14-bit rather than 10-bit you are looking at) on board too.

Kinetis L series MCUs

The LPC812 is ultra low power and has reference design with energy harvesting: Smartphone Quick-Jack solution | www.LPCware.com

Other information on it:

- OM13069 Smartphone Quick-Jack solution|NXP

- http://www.nxp.com/documents/application_note/AN11552.pdf

Regards,

David

0 件の賞賛
返信