Human fall detection using MMA8451Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Human fall detection using MMA8451Q

跳至解决方案
2,120 次查看
jeffdev
Contributor I

I have an existing wrist-worn product that uses the MMA8451Q and I would like to add human fall detection as a feature.  I've read some research papers and looked at existing products like the Philips Lifeline and all use a pendant or attach the sensor to the wait or torso.  I do not want to waste my time trying to make fall detection work on a wrist device if the false detection rate is too high.  Does anyone have any opinions or research on wrist-worn fall detectors?  Also, I saw a NXP reference manual titled MMA7260QHFDRM Human Fall Detection Using 3-Axis Accelerometer but could not find any of the sample code it mentions.  Is this manual still valid and can I get the sample code somewhere?  Is there a sample algorithm for the MMA8451Q on fall detection?  I do not believe the freefall detection interrupt is sufficient to cover human falls.

标签 (1)
0 项奖励
回复
1 解答
1,869 次查看
david_diaz
NXP Employee
NXP Employee

Hello Jeff,

In this case, the false detections might be avoided using the FF_MT_THS and FF_MT_COUNT registers from the device.

Please find more detailed description at page 32 and 33 from the datasheet.

 

If you are interested, please let me know. I will be glad to help.

 

Have a great day.

David

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,868 次查看
david_diaz
NXP Employee
NXP Employee

Hello Jeff,

In this case, I would like to recommend using one of the embedded functions included in the MMA8451Q: Freefall detection.

The detection of “Freefall” involves the monitoring of the X, Y, and Z axes for the condition where the acceleration magnitude is below a user specified threshold for a user definable amount of time. Normally, the usable threshold ranges are between ±100 mg and ±500 mg.

 

Please find attached a sample project in which an interrupt is generated when a freefall event has been detected.

 

I used the FRDM-KL25Z and CodeWarrior IDE for this project.

 

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

 

Have a great day.

David Diaz.

0 项奖励
回复
1,868 次查看
jeffdev
Contributor I

Thanks David.  My main concern is that a wrist-worn device will cause too many false detections.  I was wondering if anyone has attempted to detect falling from a wrist sensor or know of any end product I can buy to test for myself before trying to implement this.

0 项奖励
回复
1,870 次查看
david_diaz
NXP Employee
NXP Employee

Hello Jeff,

In this case, the false detections might be avoided using the FF_MT_THS and FF_MT_COUNT registers from the device.

Please find more detailed description at page 32 and 33 from the datasheet.

 

If you are interested, please let me know. I will be glad to help.

 

Have a great day.

David

0 项奖励
回复