Hi,
First, to activate the self-test by setting the ST bit in the CTRL_REG2 register (0x2B), the MMA8451Q must first be put into Standby mode by clearing the ACTIVE bit in the CTRL_REG1 register (0x2A). Then you can set the ST bit in the CTRL_REG2 register and put the part back into the Active mode by setting the ACTIVE bit in the CTRL_REG1 register
Then simply compute the difference between the acceleration output of all axes with self-test enabled (ST = 1) and disabled (ST = 0) as follows:
XST = XST_ON − XST_OFF
YST = YST_ON − YST_OFF
ZST = ZST_ON − ZST_OFF
Note that it is recommended to take several samples (e.g. 10) for each axis and average them.
If these self test responses are higher than the minimum values specified for each axis in the datasheet (Table 2), the MMA8451Q passed the self test.
Let me know if you have any other questions.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
Hi,
First, to activate the self-test by setting the ST bit in the CTRL_REG2 register (0x2B), the MMA8451Q must first be put into Standby mode by clearing the ACTIVE bit in the CTRL_REG1 register (0x2A). Then you can set the ST bit in the CTRL_REG2 register and put the part back into the Active mode by setting the ACTIVE bit in the CTRL_REG1 register
Then simply compute the difference between the acceleration output of all axes with self-test enabled (ST = 1) and disabled (ST = 0) as follows:
XST = XST_ON − XST_OFF
YST = YST_ON − YST_OFF
ZST = ZST_ON − ZST_OFF
Note that it is recommended to take several samples (e.g. 10) for each axis and average them.
If these self test responses are higher than the minimum values specified for each axis in the datasheet (Table 2), the MMA8451Q passed the self test.
Let me know if you have any other questions.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.