From a hardware point of view, let the LFA (pin 17) and LFB (pin 16) float. As described in Section 2.3.7 of the datasheet, each LF[A:B] pin will always have an impedance of approximately 500K Ohm to Vss due to the LF receiver input circuitry. The LF[A:B] pins are used by the LF receiver when the LFEN control bit is set, and are not functional when the LFEN control bit is clear. The LFEN bit is in the LFCTL1 register.
From a hardware point of view, let the LFA (pin 17) and LFB (pin 16) float. As described in Section 2.3.7 of the datasheet, each LF[A:B] pin will always have an impedance of approximately 500K Ohm to Vss due to the LF receiver input circuitry. The LF[A:B] pins are used by the LF receiver when the LFEN control bit is set, and are not functional when the LFEN control bit is clear. The LFEN bit is in the LFCTL1 register.