How to configure unused LF pins in FXTH87?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to configure unused LF pins in FXTH87?

跳至解决方案
1,911 次查看
sunrme
Contributor III

I designed TPMS sensor on FXTH87. And I don't want to use LF receiver, so I have to configure LF pins to avoid a floating input. What I have to do? leave pin not connected or connect to Vss, or something else?

Really appreciate your help.

0 项奖励
回复
1 解答
1,712 次查看
franklatona-r49
NXP Employee
NXP Employee

From a hardware point of view, let the LFA (pin 17) and LFB (pin 16) float.  As described in Section 2.3.7 of the datasheet, each LF[A:B] pin will always have an impedance of approximately 500K Ohm to Vss due to the LF receiver input circuitry.  The LF[A:B] pins are used by the LF receiver when the LFEN control bit is set, and are not functional when the LFEN control bit is clear.  The LFEN bit is in the LFCTL1 register.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,713 次查看
franklatona-r49
NXP Employee
NXP Employee

From a hardware point of view, let the LFA (pin 17) and LFB (pin 16) float.  As described in Section 2.3.7 of the datasheet, each LF[A:B] pin will always have an impedance of approximately 500K Ohm to Vss due to the LF receiver input circuitry.  The LF[A:B] pins are used by the LF receiver when the LFEN control bit is set, and are not functional when the LFEN control bit is clear.  The LFEN bit is in the LFCTL1 register.

0 项奖励
回复
1,712 次查看
sunrme
Contributor III

Hi Frank,

Thank you for your reply, I will let the LFA (pin 17) and LFB (pin 16) float.

0 项奖励
回复