How to check the spec. of KMZ49

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check the spec. of KMZ49

ソリューションへジャンプ
2,414件の閲覧回数
hyeongjinkim
Contributor I

Hi. All

I know that the minimum value for the external magnetic field strength of KMZ49.

1. Can you advise it for the test method? for example, the sensor orient position, some magnet, length from magnet, test equivements and etc. 

2. The H_ext(min) is 25kA/m. how much is the converted Gauss? is it right for the attached conversion table?

Thanks.

BR, hyeongjin kim.

0 件の賞賛
返信
1 解決策
2,395件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

First off, please note that the KMZ49 is not recommended for new design, due to limited longevity.

Usually customers are using a GAUSS-meter to measure the field strength of their target magnet.

The probe will be located, where later our crystal will be.

Normally our customers are contacting magnet suppliers and give all requirements to them.

The magnet supplier will take care that minimum field strength will match.

Yes, you can use the conversion table/tool, 25kA/m corresponds to 313,5G.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,396件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

First off, please note that the KMZ49 is not recommended for new design, due to limited longevity.

Usually customers are using a GAUSS-meter to measure the field strength of their target magnet.

The probe will be located, where later our crystal will be.

Normally our customers are contacting magnet suppliers and give all requirements to them.

The magnet supplier will take care that minimum field strength will match.

Yes, you can use the conversion table/tool, 25kA/m corresponds to 313,5G.

Best regards,

Tomas

0 件の賞賛
返信