Hi, is there a way to program TPMS sensors without BDM connector ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, is there a way to program TPMS sensors without BDM connector ?

1,283 Views
prashanthabib
Contributor I

Hello,

i want to program my FXTH87 sensor. I know the programming interface to this is BDM connector from P & E . But it requires the BDM connector along with the debugger. Is there a way to program this without having to use the BDM connector?

Labels (1)
2 Replies

1,030 Views
david_diaz
NXP Employee
NXP Employee

Hello Prashant,

Thank you very much for writing.

In this case, the FXTH87 has an S08, 8-bit microprocessor core, therefore you would require a universal BDM and CodeWarrior to program it.

I would recommend you the following BDM interface.

 

Please note that the BDM is open source, so you can implement your own programmer.

OSBDM is an open source hardware/software/firmware design which provides low-speed debug communications for different NXP processors. It is embedded within many of NXP’s development board and tower cards.

 

Please find more information at:

https://www.pemicro.com/osbdm/osbdm_description.cfm

 

I hope this information helps.

Best Regards,

David

1,030 Views
prashanthabib
Contributor I

Hello David,

Thanks for the info. 

0 Kudos
Reply